missing-QuestionPost

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! i got error as busheavy in pcan view.please help me

respected sir,i am using SPC560B54L5 and i am testing can protocol in pcan view i got error busheavy status . i am also checking on oscilloscope only getting rx signal from transceiver. CAN interface connectionis like from pcan to transceiver and tra...

0690X0000087jlSQAQ.png
ppate.16 by Associate II
  • 9263 Views
  • 3 replies
  • 0 kudos

SPC560B50L1 not working..

Hello...​have a question for SPC560B50L1. ​when put in 12V in board, MCU power 3.3V is good, & VDD_LV line is 1.27Vbut EXTAL/XTAL pin is not working......​so, i wonder if should be downloaded for the first time.when bought MCU, MCU contain basic S/W ...

LJaey by Associate
  • 316 Views
  • 0 replies
  • 0 kudos

Resolved! SPC570S50E1, Hardware error: What are the possible reasons for over current after powerring on for 1-2 minutes?

A piece of SPC570S50E1 chip is soldered on a PCB surving for its minimum system without any other component to test if it could be powerred on normally. After 3.3V/5V provided, the chip works in normal current for 1-2 min, and the 1.2V could be measu...

JW.3.262 by Associate
  • 480 Views
  • 1 replies
  • 0 kudos