cancel
Showing results for 
Search instead for 
Did you mean: 

What is there that changed in most recent (....spc574kxx_1.16.1.20210914101245) LLD release?

CoolMo
Associate III

Hi all, I got back on a project on the SPC574K2 I paused a few months ago and decided to start over from a green-field environment.

I then downloaded and installed SPC5Studio 6.0.0 Doyle which came along with version 1.16.1.20210914101245 of the LLD sdk.

Unfortunately my project builds fine but it is not running anymore due to a problem in board clock management (I', using the EVBoard)

To have proof of evidence for this I re-installed 6.0.0.Asimov (which instead comes with LLD version 1.13.1.20200626121018 with which, instead, my code (AND the EXAMPLES provided by ST) builds and runs just fine

Needless to say I'm pretty unhappy of this finding which came out without any explicit notice >:(

Has anyone run into similar issues? how did you got away?

Thanks in advance

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello CoolMo,

Update on SPC574K2 RLA has been pushed in http://download.spc5studio.com/updates

You can update only the following feature

SPC5-RLA_SPC574Kxx_Support_Feature 1.16.2

0693W00000FCcoXQAT.pngSorry for the issue ;)

Best Regards

Erwan

View solution in original post

5 REPLIES 5
Erwan YVIN
ST Employee

Hello CoolMo ,

We have well a clocking issue on K2 on Doyle

we are validating a patch and pushing a patch on SPC5RLA side asap.

http://download.spc5studio.com/updates

Best Regards

Erwan

CoolMo
Associate III

Thank you very much for a prompt reply Erwan,

I'll keep an eye on the update release.

M

Erwan YVIN
ST Employee

Hello CoolMo,

Update on SPC574K2 RLA has been pushed in http://download.spc5studio.com/updates

You can update only the following feature

SPC5-RLA_SPC574Kxx_Support_Feature 1.16.2

0693W00000FCcoXQAT.pngSorry for the issue ;)

Best Regards

Erwan

Yes, I can confirm the examples now work with 1.16.2.

Thank you for prompt and quick acting.

one last thing: signing of plugin may need to be included for next releases (install anyway is possible and things work afterwards):

0693W00000FCeDxQAL.pngThanks again

Mo

Erwan YVIN
ST Employee

Hello CoolMo ,

We need to create a real signature in our next delivery workbench. (features & plugins)

you can click on "Install Anyway"

it is a change request in our process ;)

Best Regards

Erwan