cancel
Showing results for 
Search instead for 
Did you mean: 

Using CAN on SPC560B-DIS

srosen
Associate II
Posted on November 19, 2014 at 16:24

Hello,

I am trying to make a simple project that for a start can send a single CAN frame.

I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).

I took a CAN sample  from other evb and merged it to my project but it doesn't work!

Is there any CAN sample that works that I can use?

Can I connect a scope to the TX pin and view the data without converter to CAN High and CAN Low?

In the example i did not see any initialization to the I/O (Tx and Rx) is that correct?

Can I use the external clock on my board for the CAN module?

Thanks

Shachar
11 REPLIES 11
sdesance
Associate
Posted on October 14, 2015 at 11:46

Hello Erwan,

I have the same question than other people in this post.

I want to use a CAN port with the SPC560B-DIS.

I have donloaded the ''SPC560Bxx OS-Less CAN Test Application for Discovery'' configuration that you have given in your last post and I try to configure it for use the FlexCAN0 module: I disable loopback mode, but I can't see anyt signals with my scope on TX and RX ((PB[0] and PB[1]).

My application is in attachment: can you say me what is wrong?

Thanks for your help,

Sylvain

________________

Attachments :

MX_SPC560Bxx_OS-Less_CAN_Test_Application_for_Discovery.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qZEp&d=%2Fa%2F0X0000000bp9%2FmP742HZNDYQBe9mNU8.KVIg6GPVjANfCJfai5ThgsGA&asPdf=false
Erwan YVIN
ST Employee
Posted on October 15, 2015 at 11:42

Hello Sylvain ,

i do not see any filters on your CAN configuration.

How do you check your CAN Frame transmission ?

    Best Regards

                      Erwan