cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to connect to SPC58EC-DISP board through UDE debugger.

AChie
Associate

I am trying to connect to the SPC58EC-DISP board through PLS UDE Starter kit to program and debug the Serial Test Application example provided with the SPC5 Studio IDE. After opening the debug.wsx in the example project file on PLS UDE, an error appears.(Seen in UDE error png and the connection failed report log)

I can see the devices connected through device manager as "PLS USB JTAG Adapter for SPC5xxxx A".

Please let me know why I can not connect to the boards.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
AChie
Associate

Issue resolved. Got a new board and tested against it with the same configurations and it worked. Issue was with the original board I was working with.

View solution in original post

1 REPLY 1
AChie
Associate

Issue resolved. Got a new board and tested against it with the same configurations and it worked. Issue was with the original board I was working with.