2018-10-29 10:53 AM
I am trying to connect to the SPC58EC-DISP board through PLS UDE Starter kit to program and debug the Serial Test Application example provided with the SPC5 Studio IDE. After opening the debug.wsx in the example project file on PLS UDE, an error appears.(Seen in UDE error png and the connection failed report log)
I can see the devices connected through device manager as "PLS USB JTAG Adapter for SPC5xxxx A".
Please let me know why I can not connect to the boards.
Solved! Go to Solution.
2018-10-30 6:23 AM
Issue resolved. Got a new board and tested against it with the same configurations and it worked. Issue was with the original board I was working with.
2018-10-30 6:23 AM
Issue resolved. Got a new board and tested against it with the same configurations and it worked. Issue was with the original board I was working with.