2022-10-26 12:55 AM
I want to buy jtag module
when looking for it,
Looks like I'll have to buy the SPC5-UDESTK-EVAL.
(Is that right...? anyway...)
So I'm going to buy this product, but there are SPC56 and SPC57 in the description, but there is no SPC58.
Is it right to buy this product? Or do I have to buy another product?
This is the site you want to buy.
https://www.mouser.kr/c/?q=SPC5-UDESTK
Additional question.
Does SPC5-UDEDEBG upgrade the license period and write capacity of SPC5-UDESTK-EVAL?
2022-10-26 12:59 AM
SPC5-UDESTK is the USB dongle for SPC5 debugging (suitable also for SPC58NH boards)
Please have a look here: SPC5-UDEDSTK
Best Regards.
2022-10-26 01:18 AM
2022-10-27 03:14 AM
SPC5-UDESTK-EVAL support SPC56, SPC57 and also SPC58
Yes SPC5-UDEDEBG upgrade the license period and write capacity of SPC5-UDESTK-EVAL
download software from https://www.pls-mc.com/service/downloads/download-spc5-udestk/
then look at file:///C:/Program%20Files/pls/UDE%20Starterkit%202021/release.htm
high end device like SPC58NH is supported but with following limitation:
see file:///C:/Program%20Files/pls/UDE%20Starterkit%202021/release.htm for all details
Best regards