cancel
Showing results for 
Search instead for 
Did you mean: 

This is a purchase question aoubt spc58nh-disp flash module

hans536
Associate III

I want to buy jtag module

when looking for it,

Looks like I'll have to buy the SPC5-UDESTK-EVAL.

(Is that right...? anyway...)

So I'm going to buy this product, but there are SPC56 and SPC57 in the description, but there is no SPC58.

Is it right to buy this product? Or do I have to buy another product?

This is the site you want to buy.

https://www.mouser.kr/c/?q=SPC5-UDESTK

Additional question.

Does SPC5-UDEDEBG upgrade the license period and write capacity of SPC5-UDESTK-EVAL?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
3 REPLIES 3
Giuseppe DI-GIORE
ST Employee

SPC5-UDESTK is the USB dongle for SPC5 debugging (suitable also for SPC58NH boards)

Please have a look here: SPC5-UDEDSTK

Best Regards.

hans536
Associate III

I went to the site and there is no spc5-udestk, only spc5-udestk-eval.

Can I buy this?

Gaetano SANTORO
ST Employee

SPC5-UDESTK-EVAL support SPC56, SPC57 and also SPC58

Yes SPC5-UDEDEBG upgrade the license period and write capacity of SPC5-UDESTK-EVAL

download software from https://www.pls-mc.com/service/downloads/download-spc5-udestk/

then look at file:///C:/Program%20Files/pls/UDE%20Starterkit%202021/release.htm

high end device like SPC58NH is supported but with following limitation:

  • SPC58NH84 (Cut1, only Core2)
  • SPC58NH90 (Cut1, only Core2)
  • SPC58NH92 (Cut1, Cut2, only Core2)

see file:///C:/Program%20Files/pls/UDE%20Starterkit%202021/release.htm for all details

Best regards