cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5Studio project settings

ssk
Associate II
Posted on June 18, 2015 at 12:49

Hello,

I am using SPC5Stuido and the output file is generated as out.elf or out.hex etc. It is the default setting. I want to change it as per project need. From which project settings can I change the output file name? Where is it documented?

Thanks in advance.

Mike.
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
3 REPLIES 3
Posted on June 18, 2015 at 14:35

Hi,

In the platform component, under ''Build'', there is ''Application Name''. The default is ''out''.

Giovanni

ssk
Associate II
Posted on June 18, 2015 at 16:43

Thanks Giovanni. I missed that section, was looking under project properties.

Mike.

Posted on June 18, 2015 at 17:03

In general in SPC5Studio it is better to assume that it is in the configuration. Project properties do not do much because projects are Makefile-based and the makefile is generated.

Giovanni