cancel
Showing results for 
Search instead for 
Did you mean: 

SPC58xNxx PWM Generation with TOM (AN5552 Application Note)

OrhunNiso
Associate

Hello, on SPC58xNxx board, I've been trying to generate PWM signals using Timer Output Module (TOM) and I followed this guideline:

AN5552: https://www.st.com/resource/en/application_note/dm00730101-generate-pwm-signals-with-gtm-stmicroelectronics.pdf

 

The only difference between my attempt and the guideline is that I used another TOM channel & pin to output the PWM signal. However, I cannot see any oscillation on the Logic Analyzer. I already checked the Logic Analyzer and in another project, I could see a live signal on the same pin.

 

I attached the project as zipped and I need some support about this problem.

0 REPLIES 0