cancel
Showing results for 
Search instead for 
Did you mean: 

SPC58Ex PWM setting. Someone could me help with a SPC5 Studio setup and code as well?

SGeno.1
Associate
 
2 REPLIES 2
Giuseppe DI-GIORE
ST Employee

Please have a look at SPC5Studio PWM demos.

Just for info:

SPC582B: PWM is generated using eMIOS

SPC584B: PWM is generated using eMIOS

SPC58EC: PWM is generated using eMIOS

SPC58xG: PWM is generated using eMIOS

SPC58xE: PWM is generated using GTM (install GTM plugin)

SPC58NN: PWM is generated using GTM (install GTM plugin)

Regards,

Giuseppe

SGeno.1
Associate

Hi Giuseppe.

Thanks an example installed in the SPC5 Studio "SPC58ECxx_RLA PWM-ICU Test Application" the pwm took place in my evaluation board.

SPC5 studio setting and main.c code as well, are now perfect clear.

Thank you.

Regards

Santino