cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560 Controller Board with L6230 Driver Board

Saravanan_Mari
Associate III

Hi Everyone,

    

As you know we are working on the Custom BLDC Driver Board with SPC platform in that we are facing the Some issue in the FOC integration.

Current environment and setup:

1. FOC Source code (SPC_MCTK_LIB) for SPC560p DISP Board

2. FOC source code for X-Nucleo IHM001 Board.

3. SPC560p Discovery Board

4. X-Nucleo IHM001 Board with Bull running Motor.

We are trying to replace the L9907 driver Board from the SPC_MCTK_01 kit with L6230 driver Board of X-Nucleo IHM001 Board.

Queries

1. Current FOC code Part of SPC_MCTK_01 has the L9907 driver code, We are trying to replace the l9907 driver code with L6230 driver code to suite our custom BLDC motor drive. Please guide us which and what part of the software has to be changed in order to make this integration correct.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Mari ,

Which IDE do you use for your work ?

For this work, I would use SPC5Studio 6.0.

Recreate api , internal , register from spc5xx_l9908_component_rla

Do you access to MCTK Features/plugins for SPC5Studio .

0693W000007DmZNQA0.png 

Best Regards

Erwan

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee

Hello Mari ,

Which IDE do you use for your work ?

For this work, I would use SPC5Studio 6.0.

Recreate api , internal , register from spc5xx_l9908_component_rla

Do you access to MCTK Features/plugins for SPC5Studio .

0693W000007DmZNQA0.png 

Best Regards

Erwan

Saravanan_Mari
Associate III

We are using the Same as you suggest one only(SPC studio 6.0)

In that we doesn't have the Driver layer for the L6230 driver code

I dosen't know what are the MCTK Features/plugins for SPC5Studio.

Please explain this for us to understand this deeply and moving forward..

Thanking for reply

Saravanan Mariyappan