2017-12-21 02:04 AM
Dear All ,
SPC5Studio 5.7.1 is available
*** Highlights ***
Here are the changes coming with SPC5Studio v5.7.1
For Selected Customers:
================
- Network bugs fixingUse these following update sites :
http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5
http://spc5.drive.cloudforge.com/projects/spc5tools/updates
(New update Site for free GCC feature and PLS Feature)http://hightec.spc5studio.com/
(Hightec compiler)Merry Christmas
Erwan
#spc58 #spc5studio #spc56 #spc572018-01-18 03:23 AM
PinMap editor for SPC570S50 is available?
2018-01-18 07:11 AM
Yes , it is 😉
2018-02-01 06:54 AM
it not working fine, because when I click on PinMap editor Link error message appears:
'Device specific model 'SPC570S50E1' not supported!'
2018-02-02 02:25 AM
Yes , it is supported
have you installed the last version of the pinmap ?
Cf SPC5Studio marketplace
Best regards
Erwan
2018-02-11 04:20 AM
Does SPC5 Studio support new SPC58x microcontrollers? If not is it planned to implemented support for theses controllers soon? I´ve installed the new SPC5 Studio release and would like to experience with SPC582B-DIS board.
2018-02-12 12:42 AM
Hello ,
Please refer to the installation procedure after downloading SPC5Studio
for SPC58x family ,it is for selected customers
could you send an email to
mailto:credentials@spc5studio.com
?
if the marketing guys are ok , we will send you a login/pass for spc58x support
Best regards
Erwan
2018-06-05 09:05 AM
I have the latest version of pinmap installed from the marketplace but I still have the same problem. I'm using the SPC570S-DISP eval board.
2018-06-06 02:52 AM
Hello Yalin ,
Could you try to use the official update site ?
Use these following update sites (Mass Market) :
/external-link.jspa?url=http%3A%2F%2Fspc5.drive.cloudforge.com%2Fprojects%2Fspc5releases%2FSPC5Studio%2Fupdates5
/external-link.jspa?url=http%3A%2F%2Fspc5.drive.cloudforge.com%2Fprojects%2Fspc5tools%2Fupdates
(New update Site for free GCC feature and PLS Feature)/external-link.jspa?url=http%3A%2F%2Fhightec.spc5studio.com%2F
(Hightec compiler)/external-link.jspa?url=http%3A%2F%2Fflasher.spc5studio.com
(Flasher)Anyway , update by proxy could generate some issues ?
Best regards
Erwan
2018-06-06 02:59 AM
Hi Erwan,
I am using the official update sites, as can be seen in the attachment.