cancel
Showing results for 
Search instead for 
Did you mean: 

Problem in connecting to the target SPC560Bxx Disc board

prashanth.mohan22
Associate III

0690X000008a5MpQAI.png

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello , Could you check your device manager ?

You should see PLS USB JTAG

0690X000009XiaZQAS.png

if not , install the drivers located in

c:\Program Files (x86)\pls\UDE 4.10\Driver\

Best Regards

Erwan

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee

Hello , Could you check your device manager ?

You should see PLS USB JTAG

0690X000009XiaZQAS.png

if not , install the drivers located in

c:\Program Files (x86)\pls\UDE 4.10\Driver\

Best Regards

Erwan

prashanth.mohan22
Associate III

Hi @Erwan YVIN​ ,

I've connected the device to my PC. The lights are glowing on the board, but the PC is not detecting it as USB and hence no COM ports are assigned to it. Is it a problem with the SPC560B-DIS hardware?

My other SPC560B-DIS board is working fine. Help me resolve this issue.

Regards,

Prashanth