cancel
Showing results for 
Search instead for 
Did you mean: 

Printing float, integer value

ssk
Associate II
Posted on April 29, 2015 at 08:19

How I can print float or integer values to serial port?

Is debug window access is there like 'debug.print'? If yes, how to access that? Any example for it?

Thanks.

Mike.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on April 29, 2015 at 17:38 Hello Mike , For os-less , you have to use : chnWriteTimeout(&SD1, (uint8_t *)''Hello World! '', 14, TIME_INFINITE); You have to write your own function to display an integer ;-) if you do not want to reinvent the wheel , with chibios , you can use chprintf (cf in commands of chibios)

chprintf(chp,

''%.8lx %.8lx %4lu %4lu %9s %lu

''

,
(uint32_t)tp, (uint32_t)tp->p_ctx.sp,
(uint32_t)tp->p_prio, (uint32_t)(tp->p_refs - 1),
states[tp->p_state], (uint32_t)tp->p_time);

for float : (non official)

you have : to add ''-msoft-float'' in your compiler option to emulate float by software. for Chibios , in chibios.h , #define CHPRINTF_USE_FLOAT TRUE

chprintf(chp ,

''%f''

...)

in the next releases , we will update Platform Component . Best regards Erwan