2019-05-16 12:41 AM
I try to install the SPC5-MCTK-LIB_RTM_1_1_0_web under SPC5Studio 5.8.1 according to the "Quick Start Guide Motor Control ToolKit for SPC5Studio". First I Updated the whole IDE and added the available components. Then I tried to install the MCTK-LIB.
When I reach the Steps described at Page 14 (Add local Software), I see how the IDE tries to compute alternate solutions while clicking next, where I get the following Error:
"Cannot complete the install because one or more required items could not be found.
Software being installed: SPC56xx Web Motor Control Feature 1.0.0.201807231455 (com.st.spc5.components.spc5rla.spc56xx.webmotorcontrol.feature.feature.group 1.0.0.201807231455)
Missing requirement: SPC56xx Web Motor Control Feature 1.0.0.201807231455 (com.st.spc5.components.spc5rla.spc56xx.webmotorcontrol.feature.feature.group 1.0.0.201807231455) requires 'com.st.spc5.components.spc5rla.spc5xx.full.feature.feature.group 1.5.0' but it could not be found"
Is it possible to get the MotorControl-Kit 1.1.0 working under SPC5Studio 5.8.1?
And, if yes, what am I doing wrong?
Best regards,
Adrian
Solved! Go to Solution.
2020-02-10 07:56 AM
Dear All ,
in SPC5Studio 5.8.1 :
For the MCTK backward compatibility for SPC5Studio 5.8.1
1) you should add : (Cloudforge is down)
http://mirrors.spc5studio.com/rla-mctk
2) And Install the current version of MCTK
Best regards
Erwan
2019-05-16 02:39 AM
LIKE --> the Error dissappeared and the installation is working again, seems like I need to learn more about legacy-problems, but the MCTK (1.1 is the actual Version) seems to be installed, so thanks from Germany
2019-09-02 06:02 AM
Hello,
I had the same issue and fixed it with your help, but there's another problem when trying to build the project (Regardless which of the Web Motor Control Demos I choose).
The steps I made are:
1.) Import samples from application
2.) Choose one of the motor control applications
3.) Generate the SPC5 Application
4.) Build the SPC5 Application
The last step generates following error message:
./components/spc56xx_web_motor_control_component/lib/System_Drive_Params/src/Spc5xxx_MC_it.c:48:21: fatal error: pal_lld.h: No such file or directory
#include "pal_lld.h"
Which is a bit strange, since I didn't make any changes to the configuration.
Can you please help?
2020-01-22 02:08 AM
Hi,
Did you find any solutions to this issue ?
I have the same error with SPC5-MCTK-LIB 1.1.0 and SPC5Studio 5.8.1 .
2020-02-10 07:56 AM
Dear All ,
in SPC5Studio 5.8.1 :
For the MCTK backward compatibility for SPC5Studio 5.8.1
1) you should add : (Cloudforge is down)
http://mirrors.spc5studio.com/rla-mctk
2) And Install the current version of MCTK
Best regards
Erwan
2020-09-08 01:43 AM
I have the same problem using SPC5 studio 6.0. http://mirrors.spc5studio.com/rla-mctk not working.