cancel
Showing results for 
Search instead for 
Did you mean: 

Issue in Flashing the SPC584B- DSM board

VPAI.1
Associate

Hi Team,

Please help to resolve the issue

Flashing the SPC584B- DISP board failed and end up in the following errors,  

Error messages:

 PpcJtagTargIntf: Connection to target lost !

 PpcJtagTargIntf: Failed to reset target system !

 PpcJtagTargIntf: No JTAG client found !

Please check:

- target power supply

- JTAG cable connection

- target configuration 

  • This issue has started just after connecting with external LIN device(NeoVI Blue).
  • All indicator LEDs in the board are still glowing.
  • The device is still visible in Device Manager under Ports on connecting with the computer.
  • There is no fluctuation in the current observed.
  • The power is given through regulated power supply keeping maximum current 200mA.

Regards

Sudeendra S

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Sudeendra ,

Could you install the PLS drivers located in UDE Folder

c:\Program Files (x86)\pls\UDE Starterkit 4.10\Driver\JtagUsbDriver\ ?

Best Regards

Erwan

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee

Hello Sudeendra ,

Could you install the PLS drivers located in UDE Folder

c:\Program Files (x86)\pls\UDE Starterkit 4.10\Driver\JtagUsbDriver\ ?

Best Regards

Erwan

VPAI.1
Associate

​Hi Erwan,.

Thanks allot.Resolved the issue by the suggestion provided.

Regards

Sudeendra s