2022-09-28 05:59 PM
There are several R52+ cores available in Stellar SR6 P7 line, e.g. SR6P7C8.
I have question about the Symmetric Multi-Processing (SMP) support on these R52+ cores. Is SMP available inside R52+ cluster or among R52+ clusters?
2022-10-17 02:16 AM
Hello,
SMP is a matter of Operating System.
SR6P7 devices provides support for SMP Real Time Operating Systems.
There is no MMU so Linux OS cannot be supported.
Regards,
Giuseppe
2022-11-21 01:13 AM
Thanks Giuseppe,
SMP require hardware coherent for both CPU/Core, actually I found the atomic operation issue at following page,
Do you have any idea?
Thanks
2024-10-01 07:07 AM