cancel
Showing results for 
Search instead for 
Did you mean: 

In UDE VP, I cant able to flash the elf file as the core(SPC560p) toggles between inactive and running. Can anyone help me to sort out this issue. If it is a source code issue then anyone pls suggest me how to rectify this issue. Thanks in advance.

PE.1
Associate

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

Hello,

configure the UDE debugger to connect to the device at BAM address (that is just after the reset).

It should be able to get the device back to flash-able state.

See the UDE debugger help for further details (target configuration).

Regards,

Giuseppe

View solution in original post

1 REPLY 1
Giuseppe DI-GIORE
ST Employee

Hello,

configure the UDE debugger to connect to the device at BAM address (that is just after the reset).

It should be able to get the device back to flash-able state.

See the UDE debugger help for further details (target configuration).

Regards,

Giuseppe