cancel
Showing results for 
Search instead for 
Did you mean: 

Can't connect to target with UDE 5.0

David_D
Associate II

Hi,

I am working with SPC58xx, SPC5Stuido 6.0, Windows 10 and I am trying to deploy the code onto the board with UDE 5.0.

Although I've read all the topics about these issues I still can't connect to target.

The drivers have been installed properly and the Load VCA settings are enabled.

What else can I do to make it work?

Thank you!

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
David_D
Associate II

Issue has been resolved. Micro was fitted in the incorrect position.

View solution in original post

2 REPLIES 2
David_D
Associate II

I've installed UDE 5.2 and tried with that one and still doesn't work. The adapter board is SPC58xxDPT176S. The micro is SPC58EE48E7.

The target configuration file is automatically selected in SPC5Studio 6.0 as SPC58NE84. Will this be a problem?

David_D
Associate II

Issue has been resolved. Micro was fitted in the incorrect position.