2025-12-09 6:04 PM - last edited on 2025-12-11 6:55 AM by Andrew Neil
Hi,
What is the specific corresponding relationship between the sensor’s feedback value and the actual physical value?
I also hope you can provide relevant technical parameters (such as sensitivity, zero offset) and calculation formulas for reference, so as to help us troubleshoot the problem quickly.
thank you!!
Solved! Go to Solution.
2025-12-16 1:19 AM
We suspect that there is a problem with our connection method. Could you help us assess whether there is anything wrong with the connection method?
2025-12-16 2:49 AM
@snack wrote:When the chip is shaken, the acceleration values do not change much.
Maybe that's just a false expectation of how much they should change?
Hence the recommendation to use a phone to give you some point of independent reference.
2025-12-16 2:52 AM
@snack wrote:We suspect that there is a problem with our connection method.
In that case, you would see it in the raw data.
Have you compared against a known-good implementation - such as an ST evaluation/development board?
eg, STEVAL-MKI218V1
via: https://www.st.com/en/mems-and-sensors/ais2ih.html#tools-software
2025-12-16 5:22 PM
In that case, you would see it in the raw data.
Have you compared against a known-good implementation - such as an ST evaluation/development board?
Ok, I'll try this method. Refer to the known good implementation.
Thank you very much!!