cancel
Showing results for 
Search instead for 
Did you mean: 

Why is ST introducing a new inclinometer with only 2 axis ?

Pasi MYLLYMAKI
ST Employee
 
1 ACCEPTED SOLUTION

Accepted Solutions
Carlo LARGHI
Associate III

IIS2ICLX is an inclinometer targeting top-notch accuracy and repeatability performances, and ST wanted to provide a device where all the available axes perform at best and at the same level. Considering that physical structures of the MEMS which enable in-plane sensing (so X and Y) and out-of-plane sensing (so Z axis) are different, they behaves differently in term of noise, in term of offset and offset drift, in term of frequency response and so on. So, when you buy a 3 axis device, it is not really true that you can use indifferently any axis or combine any axis because your accuracy will be anyhow limited by the worst performing axis - which is typically the out of plane one. 

View solution in original post

1 REPLY 1
Carlo LARGHI
Associate III

IIS2ICLX is an inclinometer targeting top-notch accuracy and repeatability performances, and ST wanted to provide a device where all the available axes perform at best and at the same level. Considering that physical structures of the MEMS which enable in-plane sensing (so X and Y) and out-of-plane sensing (so Z axis) are different, they behaves differently in term of noise, in term of offset and offset drift, in term of frequency response and so on. So, when you buy a 3 axis device, it is not really true that you can use indifferently any axis or combine any axis because your accuracy will be anyhow limited by the worst performing axis - which is typically the out of plane one.