2023-05-25 06:40 AM
Solved! Go to Solution.
2023-05-26 05:56 AM
Ciao @QShan.1 ,
Yes, for the LIS2DW12 is not taken into account, but considering that it is a ultra low power accelerometer, for some applications requiring low consumptions, it could be used without the IMU.
If this helps to better understand X-NUCLEO-IKS01A3 functionalities, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster.
2023-05-26 01:21 AM
Hi @QShan.1 ,
Welcome to ST Community!
It is an evaluation board system and depending on the applications there may be users who need to use only the accelerometer without having to use the IMU.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster
2023-05-26 05:17 AM
Many thanks for your answer, Federica. LIS2DW12 is a redundacy sensor. Example of Fusion9X_IKS01A3.ino does not take it in account. Is my undersatanding correct?
Qingshan
2023-05-26 05:56 AM
Ciao @QShan.1 ,
Yes, for the LIS2DW12 is not taken into account, but considering that it is a ultra low power accelerometer, for some applications requiring low consumptions, it could be used without the IMU.
If this helps to better understand X-NUCLEO-IKS01A3 functionalities, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster.