2021-12-08 6:29 PM
Solved! Go to Solution.
2021-12-09 3:00 AM
Hi @SSiow.1 ,
you can use the FP-SNS-ALLMEMS1 example that can be found in the \Projects\STM32F446RE-BlueCoin\Applications\ALLMEMS1\Binary folder. This is the STM32 ODE function pack for IoT node with BLE connectivity, digital microphone, environmental and motion sensors.
If you are using the STM32CubeProgrammer, you have to choose the .bin file with the BootLoader (BL), so the STM32F446RE-BlueCoin_ALLMEMS1_BL_vX.X.X.bin file (in DFU mode).
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-12-09 3:00 AM
Hi @SSiow.1 ,
you can use the FP-SNS-ALLMEMS1 example that can be found in the \Projects\STM32F446RE-BlueCoin\Applications\ALLMEMS1\Binary folder. This is the STM32 ODE function pack for IoT node with BLE connectivity, digital microphone, environmental and motion sensors.
If you are using the STM32CubeProgrammer, you have to choose the .bin file with the BootLoader (BL), so the STM32F446RE-BlueCoin_ALLMEMS1_BL_vX.X.X.bin file (in DFU mode).
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-12-15 2:29 AM
Hi @SSiow.1 ,
did you managed to solve your issue?
-Eleon
2021-12-15 7:33 AM
hi, yes I managed to solve it. Thank you for your help with it.
-Jet