2020-06-14 03:12 PM
I captured it when the device asked for the update but the file may have gotten corrupted. Loaded v3.41 using STLinkv2 and the sensortilebox now appears to be dead. The file I have is 726691 bytes and doesn't appear to work. Sensortile won't boot, no LEDs.
thanks,
tjm
Solved! Go to Solution.
2021-03-15 05:12 AM
2021-03-15 08:36 AM
Eleon, once again, thanks for the quick reply. Loads and runs perfectly using the STlinkV2.
I can make a connection with the application but the BlueTooth passcodes don't appear to work, 0000 or 1234. Were these changed in the latest firmware?
PS: Disregard the last BT issue, found my problem. 123456 .
Thanks,
Tony
2021-03-15 08:43 AM
Ciao Tony,
try with 123456
It's reported in the documentation but it's not a standard, let's say...
-Eleon
2021-03-15 11:13 AM
Thanks, I had found that number.
One more question. What is the designation for the battery connectors. I'd like to be able to source the connector with leads attached but I don't know the connector size or type or part number for replacement.
Thanks,
Tony
2021-03-16 01:31 AM
Hi Tony,
It is a Molex connector: you can find the component references in THIS POST, where you can also leave a like to @SGupt.4 who found the correct part number =)
-Eleon
2021-03-16 09:35 AM
Eleon, thanks once again. Checked the post and 'liked'.
Good call on checking the BOM.
For future reference, I happened to find the part number just by accident while looking over page 2 of the sensor box schematic.
Thanks,
Tony