2018-04-17 01:44 AM
From the datasheet ''..This imbalance is measured using charge integration in response to a voltage pulse applied to the capacitor.'' I would want to know at what rate this measurement is done. The maximum data rate of output to the user is 1 kHz. Which means ADC measurements performed must be at an higher rate inside the IC. Is it possible to know the sampling frequency of this internal ADC and also the type of ADC used?
Is the type of ADC used integration ADC since 'charge integration' is mentioned? More detailed explanation is required in these aspects. Please help..
https://community.st.com/tags♯/?tags=h3lis331dl%20working
‌https://community.st.com/tags♯/?tags=h3lis331dl
#h3lis331dl-working #h3lis331dlSolved! Go to Solution.
2018-04-17 03:39 AM
These information cannot be share on the forum.
2018-04-17 03:39 AM
These information cannot be share on the forum.