2019-11-04 08:09 AM
2019-12-05 02:39 AM
Hi @User_of_Sensor , sorry for the delayed answer. Please note that the Nonlinearity parameter is not commonly found in datasheets, because it is closely related to the target application. Which is yours? For a better understanding of the test, a sine vibration is applied to the DUT by sweeping in amplitude with integer step equal to 1g, from 1g to 15g and step 0.2 g from 15.2g to 16g.
Please note that these are only indicative values from characterization, since they are not in the datasheet.
Regards