cancel
Showing results for 
Search instead for 
Did you mean: 

We are using LSM6DSOX-TR Gyroscope in board. Can you suggest hardware test setup for testing Gyroscope.

ABila.2
Associate
 
2 REPLIES 2
TBomb.1
Senior II

Hi,

a standard for the Gyroscope characterization (and calibration) is the rate table, such as these ones produced by Aerosmith.

https://www.ideal-aerosmith.com/products/1-2-or-3-axis-rate-and-positioning-tables/

It is a standard in many laboratories. The main parameters to be tested are the ZRL, the noise and the sensitivity (with nonlinearities and cross-axis), and especially for this last parameter a rate table is needed.

\Tom

Thanks for reply. These look feasible during production testing. I am looking for proto board testing and reasonable cost. Can you please suggest any such.