cancel
Showing results for 
Search instead for 
Did you mean: 

We are developing an application using the A3G4250D that measures + or – 90 degrees of rotation but our accuracy/repeatability is only within +/- 1 degree, is this the expected accuracy.

RSond.2
Associate
 
1 REPLY 1
Federica Bossi
ST Employee

Hi @Community memberondraal​ ,

Welcome to ST Community!

From characterization data, this is the expected accuracy. Note that this value is based on tests on a limited sample of data and thus not guaranteed in production.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.