2020-11-15 11:30 AM
Hi,
I use 4 VL53L1X sensor with an arduino and ULD API. I set the address on 0x31, 0x33, 0x35 and 0x37..
I try to prevent a critical case which appear when one or more device are lost (timeout or hardware disconnection).
To do so, I intercept the lost of the device(s) and I reset all the address of the TOF without rebooting the Arduino with exactly the same process that was working during the first init of the ToF. But I just can see 1 device set on the address (0x29).
I have tried to restart the I2C bus with this
Someone could please let me know what to do to succeed ?
Regards,
Olivier.
2021-04-12 3:10 AM
Hi,
There is a multi sensor ranging example in released Firmware which handles 3 sensors. Please refer it.