2019-11-29 5:08 AM
I am using the function VL53L1X_SetXtalk to set the crosstalk value. When I want to read back the crosstalk value with the function VL53L1X_GetXtal, this function returns always 0.
2019-12-03 1:33 AM
I have further investigated this bug and I found out that the function VL53L1X_GetXtalk uses VL53L1_RdDWord for reading out the crosstalk value.
But what I see is that this register is only 16 bits wide. So I have changed two lines in the function VL53L1_GetXtalk and now it works:
uint16_t tmp;
status = VL53L1_RdWord(dev,ALGO__CROSSTALK_COMPENSATION_PLANE_OFFSET_KCPS,&tmp);
Could anyone else confirm this workaround?
2019-12-19 1:11 PM
The latest software in the Ultra light driver contains your fix.
I'm guessing you were not the only one to find the bug.
VL53L1X_ERROR VL53L1X_GetXtalk(uint16_t dev, uint16_t *xtalk )
{
VL53L1X_ERROR status = 0;
uint32_t tmp;
status = VL53L1_RdDWord(dev,ALGO__CROSSTALK_COMPENSATION_PLANE_OFFSET_KCPS, &tmp);
*xtalk = (uint16_t)(tmp*1000)>>9; /* * 1000 to convert kcps to cps and >> 9 (7.9 format) */
return status;
}
2020-07-20 10:20 PM
Hi Guys, a question here, i wonder if i install VL53l1X at shower room to detect falling , will it affected by steam or hot environment?
2020-07-21 9:34 AM
this is such a good question, I'm going to place it as a new query instead of putting it at the bottom a this thread.
2020-09-29 4:03 AM
Hello @John E KVAM ,
I have the same problem as @Fabian . That code doesn't work for me. After debugging and much trial and error, this is the code that works for me:
*xtalk = (uint16_t)((tmp*1000)>>25);
The reason I right shift 25 is that tmp is uint32_t and first 16 bits are zero. So 9 + 16 = 25:
tmp = b31 b30 b29 b28 b27 b26 b25 b24 b23 b22 b21 b20 b19 b18 b17 b16 0000 0000 0000 0000. Where:
Am I right?
Regards