cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L0X running on a 3.3 voltage rail

Tashfique
Associate II

We have designed a circuit using this chip with the 3.3 voltage rail . Without converting it to 2.8 as it is bellow the max thresh-hold as per the datasheet.

We also pulled up the XSHUT pin high to 3.3v using a 10k ohm resistor. In theory it should put the device into a software standby state. But the device doesn't turn on.

The only way we were able to turn on the device on was directly connecting the 3.3 v to the XSHUT pin, but it fails to do any sort of ranging.

We followed the Application schematic, described on the datasheet.

Any help will be greatly appreciated.

3 REPLIES 3
Aharon1
Associate II

any news on that issue?

Tashfique
Associate II

switched over to vl6180x and put a Voltage Regulator ...

Hardwariano
Associate III

We are using VL53L0X with 3.3 V rail and 10K pull-up resistors and it works. Perhaps its life span will be shortened.