2019-11-26 2:16 PM
2019-12-02 10:09 AM
From the user manual:
• Range Ignore Threshold
VL53L0X_CHECKENABLE_RANGE_IGNORE_THRESHOLD
Signal rate minimum threshold. Measurements with signal rates below this value are
ignored. This ensures that false measurements are not made due to reflection from the
housing.
And:
Range Ignore Threshold, Default limit state - normally disabled,
Default limit value = N x Xtalk Mcps/spad
where N = 1.5 by default
So how to set it...
The first thing you need is the crosstalk value. Crosstalk is the signal returned by the coverglass. There is a function to measure it. And the value returned is in the proper units (Xtalk in Mcps/spad)
If you don't use Xtalk, then you have a problem.
Can you measure the Xtalk and use that value, even it you never set the crosstalk again?
Generally one sets the Range Ignore to 1.5 times the crosstalk. Otherwise one might identify the coverglass as a target - which would be just wrong.
If you want to be very sensitive to targets farther away, you might want to try a lower multiplier.
If you don't use Xtalk, then try a low number - I'd say .4 kilo counts would be a first good guess.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.