2025-10-22 6:16 PM
Dear Sir,
Our project using LSM6DSO IMU to detect the position, the sensor temperature is very high after power on and Initialization, it's over 80 degree, I think it's abnormal, I attach the sch, can you give some suggestions, thanks a lot.
Solved! Go to Solution.
2025-10-28 8:08 AM
Hi @Jali ,
No, if INT2 is not used, leave it floating or connect it to ground through a resistor as per datasheet recommendations.
2025-10-23 7:40 AM
Hi @Jali ,
I confirm you that such a temperature value is abnormal. Here are some suggestions:
2025-10-23 5:14 PM
Hi Federica,
we connect the INT2 pin to vcc directly, is it right?
2025-10-28 8:08 AM
Hi @Jali ,
No, if INT2 is not used, leave it floating or connect it to ground through a resistor as per datasheet recommendations.
2025-10-28 7:17 PM
THANKS