2024-08-30 5:10 AM
I want the tap detection to work only in x axis, so I have set the TAP_Y_EN and TAP_Z_EN to 0.
But still im able to see in the logs like interrupt from z and y.
I'm using the api lsm6dso_tap_detection_on_y_set, lsm6dso_tap_detection_on_z_set and passing 0.
2024-09-01 11:14 PM
Any updates on the above query?
I want the tap detection to work only in x axis, so I have set the TAP_Y_EN and TAP_Z_EN to 0.
But still im able to see in the logs like interrupt from z and y.
I'm using the api lsm6dso_tap_detection_on_y_set, lsm6dso_tap_detection_on_z_set and passing 0.