2019-08-04 8:12 PM
<command-line>:0:0: note: this is the location of the previous definition
In file included from ../Src/TargetPlatform.c:40:0:
../Inc/sensor_service.h:74:37: error: unknown type name 'sAcceleroParam_t'
extern tBleStatus TimeDomain_Update(sAcceleroParam_t *sTimeDomain);
^~~~~~~~~~~~~~~~
../Inc/sensor_service.h:75:51: error: unknown type name 'sTimeDomainAlarm_t'
extern tBleStatus FFT_AlarmSpeedRMS_Status_Update(sTimeDomainAlarm_t *pTdAlarm, sAcceleroParam_t *sTimeDomainVal);
^~~~~~~~~~~~~~~~~~
../Inc/sensor_service.h:75:81: error: unknown type name 'sAcceleroParam_t'
extern tBleStatus FFT_AlarmSpeedRMS_Status_Update(sTimeDomainAlarm_t *pTdAlarm, sAcceleroParam_t *sTimeDomainVal);
^~~~~~~~~~~~~~~~
../Inc/sensor_service.h:76:45: error: unknown type name 'sTimeDomainAlarm_t'
extern tBleStatus FFT_AlarmAccStatus_Update(sTimeDomainAlarm_t *pTdAlarm, sAcceleroParam_t *sTimeDomainVal);
^~~~~~~~~~~~~~~~~~
../Inc/sensor_service.h:76:75: error: unknown type name 'sAcceleroParam_t'
extern tBleStatus FFT_AlarmAccStatus_Update(sTimeDomainAlarm_t *pTdAlarm, sAcceleroParam_t *sTimeDomainVal);
^~~~~~~~~~~~~~~~
../Inc/sensor_service.h:77:50: error: unknown type name 'sAxesMagResults_t'
extern tBleStatus FFT_AlarmSubrangeStatus_Update(sAxesMagResults_t *AccAxesMagResults,sFreqDomainAlarm_t *THR_Fft_Alarms, uint16_t SubrangeNum, uint16_t ActualMagSize);
^~~~~~~~~~~~~~~~~
../Inc/sensor_service.h:77:87: error: unknown type name 'sFreqDomainAlarm_t'
extern tBleStatus FFT_AlarmSubrangeStatus_Update(sAxesMagResults_t *AccAxesMagResults,sFreqDomainAlarm_t *THR_Fft_Alarms, uint16_t SubrangeNum, uint16_t ActualMagSize);
^~~~~~~~~~~~~~~~~~
make: *** [Src/subdir.mk:61: Src/TargetPlatform.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j4 all" terminated with exit code 2. Build might be incomplete.
Where might be the root cause of this problem
2019-08-04 8:20 PM
sorry i forgot to declare. Sorry