cancel
Showing results for 
Search instead for 
Did you mean: 

UNICO GUI VISUALIZATION PROBLEMS

FCern
Associate II

Hi All,

I have installed UNICO GUI 9.9.0.0 to evaluate evibrations.

I have some problems in plotting values< it seems that the graphic interface does not work correctly.

I attach an image to show you the problem.

OS: W7 PRO on Intel i3-2120 -- Integrated Video Card

0693W00000AOH8tQAH.jpgThe data are correctly acquired and saved

Thank you very much for your kind support

Ciao

Fabio

5 REPLIES 5
Eleon BORLINI
ST Employee

Hi Fabio @FCern​ 

The new Unicleo versions' drivers should be compatible with OS >= Win7.

Just for a double-check, did you enable a configuration and the Start button to start acquisition?

0693W00000AObozQAD.pngCan you see the data changing in the Data tab?

0693W00000AObsrQAD.png 

-Eleon

FCern
Associate II

Hallo Eleon,

thank you very much for your answer.

I confirm that the setting are loaded correctly and I can also see raw data in the data tab, and furthermore I can also save them in a .txt files.

I see coherent datas changing, for example, the ODR of the accelerometer. But it would be very useful for my application to evaluate also the PSD; this helps me in understanding the fundamental frequency of my vibrations. But this can be easily done only with the FFT rappresentation.

It seems to be only a visualization problem...

Thank you again for your kind support.

Ciao

Fabio

Hi Fabio @FCern​ ,

we checked on a couple of win7 setups, and I confirm the issue you reported.

I asked to our internal experts, and after some tests we conclude that yes, it can be a visualization issue, probably related to video drivers...

We are aware this is not a solution, but we suggest you to switch to win10, also because win7 is no more supported now.

By the way, thank you for having reported the issue.

-Eleon

AMárq.1
Associate

Hi Eleon, I am having the same issue on winidows 10. Do you have more information in regards to this issue?

Thanks,

Alex

Eleon BORLINI
ST Employee

Hi Alex @Alejandro Márquez​ ,

Are you able to save data in a log file, but you cannot display the chart, right?

-Eleon