2018-04-13 6:28 AM
Hello guys,
The LIS3DSH is on the development board itself, which is STM32F407G (ver MB997D). And I am using CubeMX to generate the code.
Here is the wiring
Function
LIS3DSH
Master
SDA
PA7
PINB7
SCL
PA5
PINB6
SEL/SDO
PA6
3V Pin
At first, I used these two API calls before I realised that HAL_I2C_Mem_Write and HAL_I2C_Mem_Read are the
right ones.
uint8_t slavAddr = 0x3A; //[7-bit adddress is 0001 111x]
uint8_t ID,whoAmI=0x0F;
int main(void){
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
HAL_I2C_Master_Transmit(&hi2c1,slavAddr,&whoAmI,1,100);
HAL_I2C_Master_Receive(&hi2c1,slavAddr,&ID,1,100);
while (1)
{
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Surprisingly I got the default value of Who_Am_I, 0x3F (on the watch window) with the above program. But it wouldn't get every time and realized the mistake and used theHAL_I2C_Mem_Write
and
HAL_I2C_Mem_Read functions. I still don't get the output.uint8_t slavAddr = 0x3A; //[7-bit adddress is 0001 111x]
uint8_t ID,whoAmI=0x0F;
uint8_t ctrlAddr = 0x20;
uint8_t ctrlVal = 0x17;
uint8_t xAddr[2] = {0x28,0x29};
//uint8_t yAddr[2] = {0x2A,0x2B};
//uint8_t zAddr[2] = {0x2C,0x2D};
uint8_t xVal[2],yVal[2],zVal[2];
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
//HAL_I2C_Master_Transmit(&hi2c1,slavAddr,&whoAmI,1,100);
//HAL_I2C_Master_Receive(&hi2c1,slavAddr,&ID,1,100);
HAL_I2C_Mem_Read(&hi2c1,slavAddr,whoAmI,1,&ID,1,100);
HAL_I2C_Mem_Write(&hi2c1,slavAddr,ctrlAddr,1,&ctrlVal,1,100);
HAL_I2C_Mem_Read(&hi2c1,slavAddr,xAddr[0],1,&xVal[0],1,100);
while (1)
{
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
This is my post ever on any forum. I might have missed out details
Help is appreciated.
2018-04-15 6:00 PM
I didn't check your code, just show the obvious...
uint8_t slavAddr = 0x3A; //[7-bit adddress is NOT 0001 111x]
?? in IIC you have to shift the address up one bit.HAL_I2C_Mem_Read(&hi2c1,slavAddr<<1,whoAmI,1,&ID,1,100);
2018-04-20 11:35 AM
Hello, T J..
Thanks for replying.
Here is the description of the function HAL_I2C_Master_Transmit,which mentions, that 'right shift by1' has to be done. I crossed checked with the user manual from
/**
* @param DevAddress Target device address: The device 7 bits address value
* in datasheet must be shift at right before call interface
*/
HAL_I2C_Master_Transmit(&hi2c1,slavAddr,&whoAmI,1,100);
But, here's the description of the functionHAL_I2C_Mem_Read,
which doesn't mention, that '
right shift by1
' has to be done.
/**
* @param DevAddress Target device address
*/
HAL_I2C_Mem_Read(&hi2c1,slavAddr,whoAmI,1,&ID,1,100);
Anyway, I tried with what you had suggested. I still don't get the value '0x3F' in variable 'ID'.
HAL_I2C_Mem_Read(&hi2c1,slavAddr<<1,whoAmI,1,&ID,1,100);
Like, mentioned in the question, I did get the value once when I used the following function, even though the address is not right shifted. But then when I tried again with the same function, I didn't get.
HAL_I2C_Master_Transmit(&hi2c1,slavAddr,&whoAmI,1,100);
What could be the problem?
The slave address is also correct.Pins are rightly configured and set.
Could there be any problem with clock ?. I have set the I2C clock to 400Hz. I tried 200Hz also, it didn't work either.
2018-04-20 7:46 PM
Just to be sure,
please check you have 3 connections to the chip,
Lis3dsh connections to processor
4 - I2C serial clock (SCL) to PB6
5 - GND 0V < - this may be your problem.6 - I2C serial data (SDA) to PB7Pins 4 and 6 are pulled up with 10k or 1k for fast IIC.
and you have a proper solid ground connection between the chips.
your slave address must be shifted 1 bit.
it is a simple interface to use.
PB6 I2C1_SCL
PB7 I2C1_SDA,
You need a good solid ground pin/wire.
this code works:
struct DacIIC {
uint8_t DacTxBuffer[8]; uint8_t DacRxBuffer[8]; // not used};♯ define MCP4728_DacAddress 0x60 << 1
void write4Dacs(void) {
struct DacIIC MCP4728IIC;HAL_StatusTypeDef IIC_Response;
//Channel 0 Dac0_Value = (4096 * 1) / 5; // 1VMCP4728IIC.DacTxBuffer[0] = (Dac0_Value & 0x0f00) >> 8;
MCP4728IIC.DacTxBuffer[1] = Dac0_Value & 0x00ff;//Channel 1
Dac1_Value = Dac0_Value + (4096 * 1) / 5; // 2V MCP4728IIC.DacTxBuffer[2] = (Dac1_Value & 0x0f00) >> 8; MCP4728IIC.DacTxBuffer[3] = Dac1_Value & 0x00ff;//Channel 2
Dac2_Value = Dac1_Value + (4096 * 1) / 5; // 3V MCP4728IIC.DacTxBuffer[4] = (Dac2_Value & 0x0f00) >> 8; MCP4728IIC.DacTxBuffer[5] = Dac2_Value & 0x00ff;//Channel 3
Dac3_Value = Dac2_Value + (4096 * 1) / 5; // 4V MCP4728IIC.DacTxBuffer[6] = (Dac3_Value & 0x0f00) >> 8; MCP4728IIC.DacTxBuffer[7] = Dac3_Value & 0x00ff; IIC_Response = HAL_I2C_Master_Transmit(&hi2c1, MCP4728_DacAddress, &MCP4728IIC.DacTxBuffer[0], 8, 10);}