2021-08-23 3:46 AM
Hello,
I'm trying to program the STEVAL-IDP005V2 with the stlink mini v3.
The problem is that i don't have any power on the board.
The St-Link V3 mini is powered by USB, and the power don't go to the STEVAL board.
Even when i try to power it through the IO-LINK master nothing happen.
Is this normal ?
If not, how can i solve this problem ?
Thanks ^^
2021-08-25 12:00 AM
Up !
Please guys, i need an answer ^^
I don't know well STM32 MCUs, so i need some help ^^
2021-08-25 12:11 AM
what if you show us some pictures of your wiring?
From what i quickly read in UM2566 page 49
2021-08-25 12:17 AM
The wiring is exactly as explained as in this 9 steps.
Flatwires from stlink to auxiliary board to io-link board.
Then, the power come from M12 connector.