cancel
Showing results for 
Search instead for 
Did you mean: 

STPM10 Register reverse counting

jishnu mulachan
Associate
Posted on November 22, 2017 at 06:19

   We are working with STPM10 to measure the Voltage,current,Active energy,Reactive energy and apparent energy. we are using 10W to 1KW load.with current calibration as +12% and Voltage calibration as +9%. Upto 400W load the readings are proper.but when we connect load above 400W the

active energy register (DAP),reactive energy register (DRP) is reverse counting for some case of load.kindly provide when the register is starts countdown and how can we solve this issue

thanks 

#stpm10
0 REPLIES 0