2021-02-07 5:46 AM
We purchased late in 2020 an STEVAL-STWINKT1.
Just learnt that this board has been deprecated and the STEVAL-STWIN KT1B is instead the recommended reference design
Could you please let us know:
BR
DS
Solved! Go to Solution.
2021-02-08 2:43 AM
Hi DS @dsamm ,
In general, you can indifferently use the STEVAL-STWINKT1 platform or the STEVAL-STWIN KT1B one, except in the case you want to use the new features, that are summarized as follow:
At the moment, the only software designed to run exclusively on the new STEVAL-STWIN KT1B is the FP-AI-NANOEDG1, that uses the locking mechanism for 3rd party libraries.
So, if you are using the platform regardless the hardware differences, you can safely use the STEVAL-STWINKT1.
In case this answer was helpful for you, please select it as "best".
-Eleon
2021-02-08 2:43 AM
Hi DS @dsamm ,
In general, you can indifferently use the STEVAL-STWINKT1 platform or the STEVAL-STWIN KT1B one, except in the case you want to use the new features, that are summarized as follow:
At the moment, the only software designed to run exclusively on the new STEVAL-STWIN KT1B is the FP-AI-NANOEDG1, that uses the locking mechanism for 3rd party libraries.
So, if you are using the platform regardless the hardware differences, you can safely use the STEVAL-STWINKT1.
In case this answer was helpful for you, please select it as "best".
-Eleon
2021-02-08 3:55 AM
thanks!
-daniele