2013-04-08 01:36 PM
Hi all,
I am new to the ST MEMS line, and recently purchased a few of the development boards to start testing (STEVAL MKI109V2, MKI120V1, and MKI115V1). I followed the manuals for assembly and installing Unico, and have gotten the pressure sensor board to work over USB. However, when I plug the Bluetooth module in and power up, the D2 LED on the BT module is barely lit and the device does not show up in a windows Bluetooth device scan. It seems as though there is a fault somewhere in the BT module but I figured I would ask here before trying to RMA. Thanks, Jon #steval-mki115v1