2025-01-07 5:38 AM
Hi. I have both the ST1VAFE3BX and the X-NUCLEO-IKS4A1 and I'm trying to read data from the biosensors using MEMS-studio, but I don't see how to get MEMS-studio to recognize the biosensors. The documentation for the biosensors has instructions for working with the ProfiMEMS tool (a different motherboard). In that documentation, it shows that there are biosensors. The docs for the ST1VAFE3BX also indicate that it will work with the IKS4A1 but it's not obvious to me how to make MEMS-studio "see" the biosensors as a data source.
any help would be appreicated.
TIA.
-Rich
Solved! Go to Solution.
2025-01-09 5:41 AM - edited 2025-01-09 5:42 AM
Hi @Rauscher ,
The ST1VAFE3BX + X-NUCLEO-IKS4A1 is not supported by MEMS Studio yet. If you want to see the biosensors with MEMS Studio you have to use the ST1VAFE3BX with the ProfiMEMS Tool.
2025-01-09 5:41 AM - edited 2025-01-09 5:42 AM
Hi @Rauscher ,
The ST1VAFE3BX + X-NUCLEO-IKS4A1 is not supported by MEMS Studio yet. If you want to see the biosensors with MEMS Studio you have to use the ST1VAFE3BX with the ProfiMEMS Tool.
2025-01-09 6:37 AM
Thank you, I appreciate it!