2026-05-10 12:45 PM
I am currently working on a project using Steval mkboxpro and I would like to implement BLE Mesh communication between them. I am still learning and I was wondering if you could give me some guidance or recommend resources on how to do this
Any help or advice would be greatly appreciated.
2026-05-11 5:24 AM
I having been working with the device over USB, I have strong doubts that the ST people will reply, I could be wrong, but I doubt it.
Why would you want to do such a thing, the data is tremendous, about 5 days of data from a single device is 131 GB for useful analysis. it is sitting on a separate hard drive.
2026-05-11 8:29 AM
i have a project and this is mandatory
2026-05-11 12:17 PM
I do not use BLE if I can avoid it. Sorry
2026-05-12 6:04 AM - last edited on 2026-05-12 6:17 AM by Andrew Neil
Merged with existing thread - please don't start multiple threads on the same topic.
i want to implement BLE Mesh communication between two sensorTile box pro so i flashed the fp sns blemesh1 on the card with stm32CubeProgrammer (on dfu mode) and then i used the app st ble mesh but i can't do the provisoning !!!!!
2026-05-12 6:30 AM
I am sorry, but I only have one Pro at the moment, my others are in London and it is being used in a brick experiment.
Do you get an error or nothing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.