2024-06-18 6:41 PM
When I connnect sensorTile.box from App.
the followign msg poped ip continuously. and no fucntion work properly
what is the reason. I upgraded the FW on FOTA at the first connection.
what is the suggestion ?
Thanks!
Forest
2024-06-20 12:21 AM
Hi @forest xu ,
Try to turn-off the board, unpair the SensorTile on your phone, then delete the SensorTile Bluetooth device in the phone list. Restart the board and the app on the phone.
When the pairing request appears, use the 123456 code.
2024-06-20 9:33 AM
Hi, Federica.
Thank you for your reply.
I found there is more more blue LED for BT pairing. only red LED
how can I restore to the original FW? I tried to dowload the FW from ST website
STSW-MKBOXPRO-FS, STSW-MKBOX-BLEDK
it just simply ignore my download request.
looking forward to hearing your suggestion
Thank you
Forest
2024-06-24 6:50 AM
Hi @forest xu ,
Probably after some test you need to restore the SensorTile to factory reset.
Remember to delete the Bluetooth device in the phone list before the restore, then follow this guide and check the status of SDCard by PC and the dtm.bin stored inside (formatted in FAT32) before the factory reset.
2024-06-26 11:48 PM
Hi, Federica:
Thank you for your reply.
I checked the SD card. there is no dtm.bin. there was a .Json file
so I copied the dtm.bin to the SD card and do the firmware upgrade as the picture
but I cannot connect to the SensorTile. Phone App can find it and connect to it but inside functions do not work(like the dice. motion)
PS: I restored to factory reset according to SensorTile.box PRO R2.1 Factory Reset MANUAL v0.1
Forest.
2024-07-01 5:22 AM
Hi @forest xu ,
The dtm.bin file should be copied to the sd card before performing the factory reset.
Follow the manual in the factory reset folder step by step.
This will reset the board to version 1.0.0. From there via smartphone app you can update the fw to the latest version by "BLE sensor App".
Before performing the factory reset you have to delete the sensortile from the bluetooth device list and reboot the sensortile.box.
With the original sensortile.box PRO fw you cannot use the MEMS-STudio SW (as your picture) but only the "BLE sensor app" via smartphone.