2019-10-15 7:02 AM
If you are a developer, or you are just moved by the sake of curiosity, you would desire to go deep in the functionality of the SensorTile.box, to get a full control on the platform. You will be glad to hear that ST.box is full Cube.MX compatible, so that you can create a whole project from scratch with the STCube.MX standard procedure.
From a hardware point of view, you need a programmer for STM32. While for now we suggest you the STLink V2 programmer with a custom cable, the compatibility with STLink V3 programming and debug (with level shifter to 1.8V; we suggest to use the STLink V3 mini, which is already equipped with the right cable) and the related connection cable will be available soon.
We will dive into the details step by step in the firmware and software environments of ST.box following posts. Stay tuned! :soon_arrow:
2019-10-15 7:03 AM