cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding the Lis2dtw12

ggowd.1
Associate III

Dear Sir\Madam

I have been using steval-mki190v1 (LIS2DTW12 IC), Trying to communicate through I2C with STM32F103RCT6  microcontroller in LIS2DTW12 IC by default how does it act SPI or I2C. Let me know how to configure the I2C pin configuration of LIS2DTW12 communication with the STM32F103RCT6 microcontroller.   

Best regards,

Gagan Gowda

Embedded Engineer

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ggowd.1​ ,

The i2c protocol on the LIS2DTW12 is enabled by keeping the CS pin (pin2) high. 

then, you need to send an i2c command with one of the two device address. 

the device address is either 0x30 or 0x32 and can be selected by keeping the SA0 pin (pin3) high or low respectively.

Refer to chapter 6.1.1 of the datasheet for more informations about this. 

The WHO_AM_I register reports 0x44.

For example, assuming you're using an STM32, the i2c1 interface and SA0 is low 

#define SAD 0x30

uint8_t who_am_i;

HAL_I2C_Mem_Read(&hi2c1, SAD, 0x0f, 1, &who_am_i, 1, 0xff);

For more example and reference code you can look at the official repository:

GitHub - STMicroelectronics/lis2dtw12-pid: lis2dtw12 platform independent driver based on Standard C language and compliant with MISRA standard

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Federica Bossi
ST Employee

Hi @ggowd.1​ ,

Welcome to ST Community!

Using the utility STM32CubeMX you need to select the i2c peripheral under connectivity:
_legacyfs_online_stmicro_images_0693W00000bhitYQAQ.png 

Bear in mind that you need pull-ups on the SCL and SDA lanes.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ggowd.1
Associate III

Hii Federica Bossi,

I am asking u how to configure the LIS2DTW12 sensor IC using i2c peripherals. And if I send who_i_am_register 0x0f what will be response from LIS2DTW12 sensor IC

Federica Bossi
ST Employee

Hi @ggowd.1​ ,

The i2c protocol on the LIS2DTW12 is enabled by keeping the CS pin (pin2) high. 

then, you need to send an i2c command with one of the two device address. 

the device address is either 0x30 or 0x32 and can be selected by keeping the SA0 pin (pin3) high or low respectively.

Refer to chapter 6.1.1 of the datasheet for more informations about this. 

The WHO_AM_I register reports 0x44.

For example, assuming you're using an STM32, the i2c1 interface and SA0 is low 

#define SAD 0x30

uint8_t who_am_i;

HAL_I2C_Mem_Read(&hi2c1, SAD, 0x0f, 1, &who_am_i, 1, 0xff);

For more example and reference code you can look at the official repository:

GitHub - STMicroelectronics/lis2dtw12-pid: lis2dtw12 platform independent driver based on Standard C language and compliant with MISRA standard

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ggowd.1
Associate III

Hii Federica Bossi,

I would like to configure for z axis acceleration in LIS2DTW12 IC and read the data in FIFO mode. Kindly take a look at the below code for which i have configured as FIFO mode and 5 samples of data in that. let me know any correction!

int main() 

{

InitialiseHardware();

InitialiseModules();             

whoamI = I2C1_ReadRegister(who_i_am);  /* Check device ID */

if(whoamI != LIS2DTW12_ID)

while (1) {

   /* manage here device not found */

  }

// v1 = I2C1_ReadRegister(0x21);

I2C_WriteRegister(SLAVE_ADDR, 0x20, 0x60); /* set ODR 4000hz in ctrl1*/

I2C_WriteRegister(SLAVE_ADDR, 0x25, 0x10); /* set 4g in ctrl6 */

I2C_WriteRegister(SLAVE_ADDR, 0x2E, 0x25); /* fifo mode and 5 samples */

// reg.fth = 10;

//lis2dtw12_full_scale_set(&dev_ctx, LIS2DTW12_2g);

// lis2dtw12_filter_path_set(&dev_ctx, LIS2DTW12_LPF_ON_OUT);

/* Infinite loop */

while(1)

{

I2C_WriteRegister(SLAVE_ADDR, 0x2E, 0x25); /* fifo mode */

out_t_z_l_data = I2C1_ReadRegister(0x2C);

out_t_z_h_data = I2C1_ReadRegister(0x2D);

z =(int16_t)(out_t_z_h_data << 8) | out_t_z_l_data;

z_g[index] = z * (4.0 / 32768.0 );

index++;

if(index >= 5)

{

index=0;

for(fl_i = 0; fl_i >= 32 ; fl_i++)

{

z_g[fl_i] = 0;

}

I2C_WriteRegister(SLAVE_ADDR, 0x2E, 0x00); /* fifo mode */

I2C_WriteRegister(SLAVE_ADDR, 0x2E, 0x25); /* fifo mode */

}