2019-10-04 8:40 AM
Regarding steval-mki176v1 LSM6DS3H :
1) What are the specs of the internal clock for the gyro if you were spec-ing it like a crystal? What is the drift and drift with temperature?
2) Does it have an LED to show bus activity when querying the gyro or accel registers?
Thank you.
2019-10-07 7:09 AM
Hi @Roumen K , please find my answers here below:
Regards
2019-10-07 12:09 PM
2019-10-07 12:10 PM
2019-10-07 12:46 PM
I would like to re-ask the first question: if we were to set up the accelerometer up to run at 204 Hz or 25 Hz, and we wanted to know what rate the accelerometer data interrupt line would fire at, how can we spec that? Ex: 204 Hz +\- 5% across the operating temperature range or 204 Hz +\- 2% at 25C . Thank you.
2019-10-21 8:23 AM
Hi @Roumen K , 204 Hz +\- 5% should be a likely value. Regards