cancel
Showing results for 
Search instead for 
Did you mean: 

Question from Predictive Maintenance Webinar 29th of April: How to show real time fft graph using stwink1 kit?

Pasi MYLLYMAKI
ST Employee
 
1 REPLY 1
Vladimir  JANOUSEK
Associate II

STSW-STWINKT01 includes microphone ultrasound FFT SW example and PC GUI to display the FFT data. 

FP-IND-PREDMNT1 BLE example provides ISM330DHCX FFT data of accelerometer into ST BLE sensor app. There are limitations in the speed of FFT refresh rate on phone side though.

FP-IND-PREDMNT1 WIFI example (with separate WIFI extension) provides FFT data for IIS3DWB accelerometer into the ST Cloud Dashboard.

FP-IND-PREDMNT1 includes the MotionSP middleware making the FFT calculations that can be then easily re-used in own application.

Another option still is to use STEVAL-109V3 ProfiMEMS tool and IIS3DWB adapter board + UNICO GUI where FFT is calculated in the PC and displayed real-time.