2020-05-12 12:06 AM
Hello all,
I have a problem when I try to use VL53L0X GUI application: it doesn't recognize the NUCLEO-L476RG board.
First, I install STSW-LINK007 and STSW-LINK009 as manual says.
Then I connect X-NUCLEO-53L0A1 + NUCLEO-L476RG to my USB port, start the application and get the next error:
Why is this happening? Does VL53L0X GUI only works with NUCLEO-F401RE but not with NUCLEO-L476RG?
Note: I know my NUCLEO-L476RG and my X-NUCLEO-53L0A1 aren't damaged because I can download the VL53L0X examples and they work well:
Thanks in advance.
Regards.
Solved! Go to Solution.
2021-02-10 08:36 AM
2021-02-10 09:59 AM
2021-02-10 10:31 AM
2021-02-11 10:37 AM
Duane -
On a whim, I started putting the expansion board on several different Nucleo F401RE boards. Some of which I have abused quite badly.
I found 1 that had your symptom
So try this:
Use Tera Term, use 406800 as a baud rate. issue the command: (commands will NOT echo, backspace does not work)
sensors
You should get "sensor PE"
enable
You should get a lot of data.
help - lots of text
But based on your symptoms, I think you need a new NucleoF401RE board.
sorry about that.
(Actually I've only heard of one failure. It's very rare."
The enable command should generate data.