cancel
Showing results for 
Search instead for 
Did you mean: 

Maximum Distance at which the LIS2MDL sensor can detect a metal or magnet for deviation in raw data?

BRaj_48
Associate II
 
7 REPLIES 7
Ozone
Lead II

Your question has too much unefined variables.

The LIS2MDL does not detect "metal" or "magnets", but magnetic fields.

The field change caused by the object must at least exceed the noise threshold to be detectable.

BRaj_48
Associate II

Is the principle same for all the magnetometer sensor?

BRaj_48
Associate II

And how to find the range (distance) of magnetic field change of the sensor?

As always. Apply a reference signal (field of known size), and observe the sensor output.

Using geometry and the sensor datasheet (full scale range), you can calculate expected data.

BRaj_48
Associate II

I will look into it, Thank you!!!!!

Or you can trust the datasheet, and assume the LIS3MDL conforms to the given specifications.

BRaj_48
Associate II

Already I have worked on two other magnetometer sensor and the output obtained was still not as so close to the specs provided by the datasheet